Add Asset

You can add assets directly under the Site, or Area, or Sub area. Perform the following steps to add assets to the hierarchy list:
  1. Click
    Configuration
    >
    Asset setup
    from the menu bar
  2. Click the [] icon from the Site, or Area, or Sub area in the hierarchy list and select [Add node].
  3. In the
    Add node
    window, set these parameters:
    • Select item type
      : Select the
      Asset
      radio button in the left pane.
    • Name
      : Provide the node name.
    • Description
      : Provide the description of the node.
    • Functional Location
      : Provide the location details.
      NOTE: Select the
      Auto generate
      check box to use the system-generated functional location.
    • Configuration Status
      : Select the status from the drop-down list.
    • Asset Class
      : Select the asset class from the drop-down list.
  4. Click [Add].
    Add Asset
    The "
    Asset is added under the Site, or Area, or Sub area successfully
    " message displays.
  5. (Optional) In the
    Info
    tab, click [Edit] and perform the following actions:
    • Geographical Location
      : Provide the geographical location.
    • Contact Details
      : Provide the contact details.
    • Remarks
      : Provide the remarks.
    • Make
      : Provide the asset make details
    • Commission Date
      : Select the commission date using the date picker.
    • Lifecycle Status
      : Select the lifecycle status from the drop-down list.
    • Files Uploaded
      : Click [Browse] to upload the files related to the asset.
    • Click [Save].
To configure
KPI
and
Sensors
tab, see Configure KPI and Configure Sensors
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal