Enable HART invalid (output devices)

Enable HART is selected. To enable HART, these parameters must be set to the corresponding values:
  • Output Type = Current (mA)
  • Output Range = 4 mA to 20 mA
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal