Device Diagnostics parameters
Device Diagnostics
includes these parameters:Parameter | Description | Value |
|---|---|---|
Run mode | Shows the operating state for the device. Run mode is blank when the device is offline, or when the connection is not established to the device. |
|
Diagnostics thresholds exceeded | Shows whether any diagnostics are active or a threshold has been reached when the event occurred. |
|
Diagnostics sequence count | Shows the count for each time a distinct diagnostic condition was detected, and also each time a distinct diagnostic condition transitioned from detected to not detected. | 0 to 255 |
Self test | Shows whether the product initialization code detected an error. |
|
CPU utilization | Shows the usage of the compute engine. | 0% to 100% |
Chassis status | Shows whether the end cap and the device bases are properly connected. |
|
Connections | Shows the number of CIP connections currently open to and through the adapter. | 0 to 32767 |
Packets lost | Shows the running sum of the number of Sequenced Address Item Sequence Numbers that are skipped in Class 0 and Class 1 connections consumed by the adapter and its children. | 0 to 2147483647 |
Timeout | Shows the running count of the number of connections that time out, both originated and targeted, to and through the adapter. | 0 to 2147483647 |
HMI packet rate | Shows the rate at which the HMI sent data. The number of Class 3 packets and unconnected packets sent and received by the device in the previous second. | 0 to 2147483647 |
IO packet rate | Shows the rate at which the I/O sent data. The number of Class 0 and Class 1 packets that were transmitted or received by the adapter in the previous second. | 0 to 2147483647 |
Ethernet errors | Shows the sum over all ports of the following Ethernet Link object values: In Discards, In Errors, In Unknown Protos, Out Discards, Out Errors, Alignment Errors, FCS Errors, Single Collisions, Multiple Collisions, SQE Test Errors, Deferred Transmissions, Late Collisions, Excessive Collisions, MAC Transmit Errors, Carrier Sense Errors, Frame Too Long, and MAC Receive Errors. | 0 to 2147483647 |
Time synchronization - Status | Shows whether the device is currently synchronized with a 1588 master. |
|
Grand master clock identity | Shows the identity of the Grand Master clock to which the device is synced. | 8-byte hex number |
Local clock offset to system time | Shows the offset, in nanoseconds, from the local clock to the system time. Use this value to detect steps in time. This value updates when a Precision Time Protocol (PTP) update message is received. | -9223372036854775808 to 9223372036854775807 |
Local clock offset timestamp | Shows the timestamp of the local clock offset in YYYY-MM-DD-HH:mm:SS.mmm format.
| A valid time or None if no event time was recorded. |
Low System Power Alarm | Shows whether the input system power voltage has moved below the configured Low System Power Limit. If it is below the configured Low System Power Limit, it remains set until the input system power voltage moves above the configured Low System Power Alarm Limit. |
|
Low System Power Timestamp | Shows the time when a Low System Power condition most recently transitioned from No to Yes. | A valid time or None if no event time was recorded. |
High System Power Alarm | Shows whether the input system power voltage moves above the configured High System Power Limit. If it is above the configured High System Power Limit, it remains set until the input system power voltage moves below the configured High System Power Alarm Limit. |
|
High System Power Timestamp | Shows the time when a High System Power condition most recently transitioned from No to Yes. | A valid time or None if no event time was recorded. |
Over Temperature | Shows whether the product temperature is higher than its rated operating limits. |
|
Over Temperature Timestamp | Shows the time when the product most recently became higher temperature than its operating limits. | A valid time or None if no event time was recorded. |
Critical Temperature | Shows whether the product is above critical temperature limit for proper operation and may shutdown without further warning. |
|
Critical Temperature Timestamp | Shows the time when the device temperature most recently transitioned above the Critical Temperature. | A valid time or None if no event time was recorded. |
Internal Fault | Shows whether one or more of several internal diagnostics indicate an internal issue in the product. |
|
Internal Fault Timestamp | Shows the time when an Internal Fault condition most recently transitioned from false to true. | A valid time or None if no event time was recorded. |
Retry communication | Updates the data displayed in the dialog box. |
Provide Feedback