NAT view parameters
The
NAT
view includes these parameters:Parameter | Description |
|---|---|
Network Address Translation (NAT) Instances | |
Instance Name | Displays the unique name of the NAT instance. |
Gi1/1 VLAN's | Displays the VLANs assigned to the NAT instance on port Gi1/1. |
Gi1/2 VLAN's | Displays the VLANs assigned to the NAT instance on port Gi1/2. |
Gi1/3 VLAN's | Displays the VLANs assigned to the NAT instance on port Gi1/3. |
Gi1/4 VLAN's | Displays the VLANs assigned to the NAT instance on port Gi1/4. |
Diagnostics | Opens NAT Diagnostics to view diagnostic information about an instance. |
Global Diagnostics | |
Current Active Translations | Displays the total number of translations that occurred within the last 90 seconds across all NAT instances. |
Total Translations | Displays the total number of translation across all NAT instances. |
Total Translated Packets | Displays the total number of translations across all NAT instances. |
Total Untranslated Packets | Displays the total number of packets that have been bypassed and dropped across all NAT instances. |
![]() | Opens Add/Edit NAT Instance to create a NAT instance. |
![]() | Opens Add/Edit NAT Instance to edit the configuration of a NAT instance. |
![]() | Deletes the NAT instance. When the NAT instance is deleted, all of the translation parameters associated with the NAT instance are also deleted. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter password dialog box may appear. |
Provide Feedback