DHCP Address Assignment view parameters
The
DHCP Address Assignment
view includes these parameters:
TIP:
If you delete all of the rows or pools in this view and select
Refresh
, the Pool
name becomes empty.Parameter | Description |
|---|---|
Port | Displays the ports available for the configuration. For example, Gi1/1, Gi1/2, Fa1/1, Fa1/2. |
Pool | Specifies the pool names from the DHCP IP address pool that corresponds to the instances available in the switch. |
IP Address | Specifies the IP address assigned to the switch port. The format is a 32-bit numeric address written as four numbers separated by periods (for example, 255.255.255.255). The number range is between 0 and 255 (from 1 through 244). The IP address that you assign is reserved for the selected port and is not available for normal DHCP dynamic assignment. The IP address must be an address from the pool specified in the DHCP Pool field. |
Refresh | Retrieves and displays the latest values from the device. |
Set | Sends the settings to the switch. The Enter Password dialog box may appear. |
Provide Feedback