Diagnose a problem with a point
Use
Ptxx Diagnostics
to view the diagnostics information for an individual point. Diagnostics is disabled when:- You are operating offline.
- An Identity mismatch exists.
To diagnose a problem with a point
- On the tab for the device, selectPoints.
- In thePointsview, in theDiagnosticscolumn for the point, select
. - InPtxx Diagnostics, view the diagnostics for the point.
Provide Feedback