Configuration, Device Definition Bumpy Confirmation dialog box

Controller operation in multi-controller systems may be affected because a change was made to the device configuration or the device definition.
You may select
Inhibit Module
to inhibit the device before applying these changes. If this connection is an Exclusive Owner or Input Only connection and you inhibit the device, any Listen Only connections from other controllers cannot open until the connection is re-established (preventing them from misinterpreting data received from the newly reconfigured device.)
  • Select
    Yes
    to apply the changes. This may affect other controllers.
  • Select
    No
    to return to the editing session (any profile changes are pending).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal