Status desc
Displays the status of the module.
- Standby.A transient state that occurs when shutting down the connection to the module.
- Faulted.The controller is unable to communicate with the module. When the status is Faulted,Connectiondisplays the fault.
- Validating.A transient state that occurs before connecting to the module.
- Connecting.A state that occurs when establishing a connection with the module.
- Running.The module is communicating and everything is working as expected.
- Shutting down.The connections to the module are closing.
- Inhibited.The connection to the module is inhibited.
- Waiting.A connection to this module was not made because:Its parent has not yet made a connection to it.Its parent is inhibited.Its parent is faulted.
- Offline.You are not online with the controller.
Provide Feedback