Overview view parameters
The
Overview
view includes these parameters.
TIP:
Some parameters in the
Overview
view are not available for all device types.Parameter | Description |
|---|---|
Device type | Displays the device catalog number and type. |
Vendor | Displays the device manufacturer information. |
Description | Displays the device description. |
Series | Displays the device series. |
Revision | Displays the device major and minor revisions. |
Electronic keying | Displays the electronic keying used for the device. Electronic keying compares the device defined in the project to the installed device. If keying fails, a fault occurs. Valid values include:
For detailed information on Electronic keying, see Electronic Keying in Logix5000 Control Systems Application Technique, publication LOGIX-AT001. |
Connection | Displays the Connection Type and the Communication Format. |
Input Data / Output Data | Displays the input or output data type for the device. |
Data Format | Displays the type of data transferred between the device and controller. |
Counters | Displays the counter number for the device. |
Device definition | Opens Device definition to change the revision, electronic keying, and other device specific values. |
Provide Feedback