Add a controller

Add a controller to a project to connect the controller with the project. Add controllers from the
Devices
explorer.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    explorer, select Hamburger Menu Icon
    Hamburger Menu
    , then select Add device icon
    New device
    . The
    Add device to project
    dialog opens.
  3. In the
    Add devices to project
    dialog, under
    Category filter
    , select
    Controller
    .
  4. Select a controller from the list and then select
    Continue
    .
  5. Under
    Pending to configure
    , enter the controller information and then select
    Finish
    to add the controller to the device list.
    TIPP: Controller names:
    • Can contain up to 40 valid characters.
    • Can contain only alphanumeric characters and underscores.
    • Must begin with a letter or underscore.
    • Cannot include consecutive underscores.
    • Cannot end with an underscore.
    TIPP: Additional options to add a controller from either the:
    • Device list
      , at the top of the
      Device list
      , select Add Device icon
      Add device
      .
    • Execution
      explorer Execution icon. Select Hamburger Menu Icon
      Hamburger Menu
      , and then select
      Add controller
      . In the
      Add controllers to project
      dialog, select a controller from the catalog list.
Rückmeldung geben
Haben Sie Fragen oder Feedback zu dieser Dokumentation? Bitte geben Sie hier Ihr Feedback ab.
Normal