Loading

Presentation

Energy Savings with Variable Frequency Drives in Process Applications

See how use of a PowerFlex® smart VFD rather than a traditional flow valve to control the flow of a pump can result in energy savings of up to 75%. Applications using multiple motors can significantly reduce energy costs. Our industry partner Endress+Hauser helps complete the solution.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.