Loading

FactoryTalk ResilientEdge

Unlock the power of cloud intelligence and the resiliency of edge execution to keep your operations running when it counts. Discover how the FactoryTalk® ResilientEdge™ solution serving as the edge execution layer for Plex MES, enables production continuity, while accelerating enterprise scalability and performance.

What is FactoryTalk ResilientEdge?

FactoryTalk ResilientEdge is an MES edge solution that extends cloud-based manufacturing execution to the edge, combining the speed, security and reliability of low-latency MES with seamless cloud synchronization.

Benefits of FactoryTalk ResilientEdge

 
People group gear management icon

Lower cost of ownership

Modern, container-based architecture lowers maintenance and upgrade costs while freeing IT resources.

worker with hard hat and a computer screen

Accelerate time to value

With rapid deployment options, you can get up and running and start seeing ROI benefits quickly.

Speech bubbles

Scale with ease

Centralized management and monitoring accelerate deployments and simplify operations at scale.

FactoryTalk ResilientEdge Capabilities

Unlock autonomous operations

FactoryTalk ResilientEdge is an MES edge solution that delivers continuous, local execution at the edge – while securely synchronizing data flows with the cloud. The scalable architecture builds a strong foundation for advanced AI and automation initiatives – enabling manufacturers to pave the path towards autonomy.

Reduce total cost of ownership

Built on a modern architecture with centralized monitoring, and scalable modularity, FactoryTalk ResilientEdge reduces overhead costs while enabling faster deployments, simpler upgrades, and easy lifecycle management across the enterprise.

Bridge the IT and OT gap

Leveraging the FactoryTalk® Optix™ HMI platform, the FactoryTalk ResilientEdge solution extends manufacturing execution system (MES) capabilities directly into the plant-floor OT environment—enabling real-time insights through a unified operator experience.

Enable an elastic and scalable layer 

FactoryTalk ResilientEdge solution confirms production runs consistently at the edge and in the cloud, extending the elastic MES architecture of Rockwell Automation to unify operations across multiple sites, while keeping local systems running and visible at the enterprise level.

Drive high throughput automation

Built for always-on, highly automated environments, FactoryTalk ResilientEdge enables continuous execution at the edge, minimizing latency even during network disruptions. The result is faster production cycles, higher throughput, and resilient automation that keeps operations running 24/7.

Stay ahead of cybersecurity risks

FactoryTalk ResilientEdge delivers security that is built in—not bolted on. A standardized, centrally governed architecture enables manufacturers to keep pace with evolving policies, compliance requirements, and security threats—without disrupting operations.

FactoryTalk ResilientEdge In Action

See how a unified edge-to-cloud execution layer for Plex MES combines the scalability and agility of the cloud with deterministic, secure plant-level control at the edge.

Edge-to-cloud solution aligned with extreme precision to the pillars of Smart Manufacturing.

FactoryTalk ResilientEdge is designed to provide immediate value for your company, while preparing you for whatever tomorrow brings.

What is Smart Manufacturing?
Medalha de bronze

Connect

Connect your people, machines, and systems across IT and OT with secure, scalable edge‑to‑cloud data flows that unify operations from the plant floor to enterprise.

Automate icon

Automate

Automate your operational ecosystem with edge intelligence and cloud orchestration—reducing manual errors, increasing data reliability, and keeping manufacturing running with precision.

Target icon

Track

Track every event, material movement, machine state, and quality check at the edge, then unify that contextualized data in the cloud to enable enterprise‑wide visibility and control.

Analyze icon

Analyze

Analyze operational insights to optimize performance, identify emerging trends, and predict issues before they impact production - turning visibility into intelligent decision-making.

FactoryTalk ResilientEdge Features

Unified edge execution

The FactoryTalk ResilientEdge solution runs manufacturing execution locally, eliminating reliance on fragile gateways and fragmented systems - delivering predictable, high-performance operations without any compromise.


Intelligent and seamless data synchronization

FactoryTalk ResilientEdge solution securely synchronizes production data between edge and cloud—confirming continuous data flow, preserving operational integrity, and maintaining a trusted system of record ready for enterprise visibility and analytics.


Centralized monitoring and lifecycle management

The FactoryTalk ResilientEdge solution lowers lifecycle costs and accelerates deployment by reducing integration complexity, centralizing monitoring, and supporting modular scalability aligned with phased modernization strategies.


Built-in security by design

Built with a security‑first architecture that helps protect data and operations across edge and cloud environments, the FactoryTalk ResilientEdge solution keeps systems current with evolving security requirements, helping manufacturers reduce risk and maintain a modern, compliant operational footprint.

Featured Resources

FactoryTalk ResilientEdge at ROK Studios

Tune in to this interview with Rockwell Automation Senior Product Manager Hayden Foot hear about how to drive continuity and minimize the impact of disruptions with FactoryTalk ResilientEdge.

White Paper: From Automation to Autonomy
From Automation to Autonomy: The Missing Edge Layer in MES

Uncover the critical role an industrial-grade edge-to-cloud execution layer plays by operating seamlessly, regardless of connectivity issues, unplanned downtime, or other technology challenges that may arise.

Learn More
Accelerate innovation with Elastic MES - Illustration
Accelerate innovation with Elastic MES

In this four-part webinar series, we will explore how an elastic MES solution from Rockwell Automation expands beyond traditional MES to support your journey toward autonomy.

Learn More