Create a subscription

You create a subscription inside the
Start()
method.
MANCIA:
To automatically insert a new method:
  • In Visual Studio, place the caret after the
    +=
    operator, and press
    TAB
    twice.
  • In Visual Studio Code, refer to the editor suggestions.

Example

In this example, the
Session_UserChange
method is subscribed to the user change event using the
UserChange
event handler and the
+=
operator.
public override void Start() { Session.UserChange += Session_UserChange; }
IMPORTANTE: Always cancel the subscription in the
Stop()
method to avoid a memory leak. See Cancel a subscription.
The following example shows the
Session_UserChange
method.
private void Session_UserChange(object sender, UserChangeEventArgs e) { Log.Info(e.newUser.BrowseName); }
sender
The
IUAObject
object that corresponds to the node origin of the event.
e
The C# object that contains the event data based on the data type of the event handler (
UserChangeEventArgs
in the example).

Event handlers

Depending on the event type, create a subscription by using different event handlers.
Value change of a variable event
To subscribe a method to the value change of a variable, use the
VariableChange
event handler, supplied by the
IUAVariable
class. See IUAVariable.VariableChange.
All events generated by an object
To subscribe a method to all events generated by an object, use the
UAEvent
event handler, supplied by the
IUAObject
class. See IUAObject.UAEvent.
A specific event of an object
To subscribe a method to a specific event generated by an object, use the corresponding event handler supplied by the type. For more information about type event handlers, see Riferimenti oggetto e variabile.
In this example, the
OnMouseClick
event handler runs the
Button2_OnMouseClick
method each time
Button2
is pressed. The
OnMouseClick
event handler is supplied by the
Button
class.
public override void Start() { var button2 = Owner.Get<Button>("Button2"); button2.OnMouseClick += Button2_OnMouseClick; } private void Button2_OnMouseClick(object sender, MouseClickEvent e) { var label2 = Owner.Get<Label>("Label2"); var button = (Button)sender; label2.Text = "Mouse click event on " + button.BrowseName; }
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.