Develop a login page
Develop a login page that handles correct and incorrect login attempts.
Application example
![](/content/dam/dita/it/factorytalk-optix/1-00/_images/login-form.png/_jcr_content/renditions/original)
MANCIA:
You can download a sample project from:
ExampleApplication-LoginPage.zipPrerequisites:
In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select ![Run](/content/dam/dita/it/factorytalk-optix/1-00/_images/toolbar_run_icon.png/_jcr_content/renditions/original)
Fornire un feedback