IUANode.GetObject(browsePath)

Returns an
IUAObject
C# object that corresponds to the first child object of the node on which the method is invoked. The returned object name corresponds to the argument.
IUAObject GetObject(string
browsePath
);

Arguments

browsePath
(string)
Can be either:
  • The
    BrowseName
    of the object
  • The path of the object in the information model, uniquely expressed as a sequence of
    BrowseName
    values separated by
    /

Returns

IUAObject
A C# object that matches the requested object.

Examples

The following examples show a returned C# object that corresponds to the
Motor1
object:
var motor1 = Owner.GetObject("Machine1").GetObject("Motor1");
var motor1 = Owner.GetObject("Machine1/Motor1");
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.