Add users

Add users with different locales.
Prerequisites:
  1. In the
    Project view
    pane, expand the
    Security
    folder.
  2. Create two users by right-clicking the
    Users
    folder and selecting
    New
    User
    .
  3. Rename the users by hovering-over each user, selecting
    Edit
    , and entering:
    • Alice
    • Tim
  4. In the
    Project view
    pane, select
    Alice
    .
  5. In the
    Properties
    pane, set the
    LocaleIds
    property value to
    it-IT
    .
Fornire un feedback
Hai domande o feedback su questa documentazione? invia il tuo feedback qui.