The Real Time Sample (RTS) period is too low.
    The following table indicates the minimum RTS value (in milliseconds) that you can enter for the 1756-IF16 and 1756-IF8 modules, based on the Module Filter value.
| Module Filter Value | Module Filter Integer | Floating Point | ||||
| Single | Diff | HS | Single | Diff | HS | |
| 10 Hz | 488 | 244 | 122 | 488 | 244 | 122 | 
| 50 Hz | 88 | 44 | 22 | 88 | 44 | 22 | 
| 60 Hz | 88 | 44 | 22 | 88 | 44 | 22 | 
| 100 Hz | 56 | 28 | 14 | 56 | 28 | 14 | 
| 250 Hz | 28 | 14 | 7 | 28 | 14 | 7 | 
| 1000 Hz | 16 | 8 | 5 | 18 | 11 | 6 | 
where:
Single = Single-ended mode
Diff = Differential mode
HS = High-speed mode
For example, for a Module Filter value of 10 Hz on an IF16 module in Integer Single-ended mode, the minimum RTS value is 488 ms.
Provide Feedback