Low Low Alarm greater than Low Alarm
    The Low Low Alarm is greater than the Low Alarm. Enter a new Low Low Alarm that is less than the Low Alarm.
- The Low Low Alarm is the level of input to a channel that will cause the module to indicate a low low alarm. The alarm will remain until input returns above this level, unless it is within the deadband, or as long as the alarm is latched.moduleA device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
- The Low Alarm is the level of input on a channel that will cause the module to enable the low alarm. The alarm will remain until the input returns above this level, unless it is within the deadband, or as long as the alarm is latched.
Provide Feedback