Convert to BCD (TO_BCD)
    This table lists the controllers and applications that support this instruction.
            
  
    
| Architecture | Standard applications | Safety applications | 
|---|---|---|
| CompactLogix 5370, ControlLogix 5570, Compact GuardLogix 5370, and GuardLogix 5570 controllers | Yes | No | 
| CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Yes | Yes | 
The TO_BCD instruction converts a decimal value (0  Source
 Source  99,999,999) to a BCD value and stores the result in the Destination.
 99,999,999) to a BCD value and stores the result in the Destination.
 Source
 Source  99,999,999) to a BCD value and stores the result in the Destination.
 99,999,999) to a BCD value and stores the result in the Destination.
     TIP: 
    In Logix Designer version 36, the mnemonic for this instruction changed from TOD to TO_BCD.
Available Languages
Ladder Diagram

Function Block Diagram
Function Block Diagram supports these elements:
FBD Block

Structured Text
This instruction is not available in structured text.
Operands
     IMPORTANT: 
    Unexpected operation may occur if:
          
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions. 
Ladder Diagram
| Operand | Data Type CompactLogix5370, ControlLogix5570, Compact GuardLogix5370, and GuardLogix5570 controllers | Data Type CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Format | Description | 
| Source | SINT INT DINT | SINT INT DINT LINT USINT UINT UDINT ULINT | Immediate tag | Value to convert to BCD 0   Source  99,999,999 | 
| Destination | SINT INT DINT | SINT INT DINT LINT USINT UINT UDINT ULINT | tag | Tag to store the result | 
Function Block Diagram
FBD Block
| Operand | Type | Format | Description | 
| TO_BCD tag | FBD_CONVERT | Structure | TO_BCD structure | 
FBD_CONVERT Structure
| Input Member | Data Type | Description | 
| EnableIn | BOOL | Enable input. If cleared, the instruction does not execute and outputs are not updated.
                   Default is set. | 
| Source | DINT | Input to the conversion instruction.
                   Valid = any integer | 
| Output Member | Data Type | Description | 
| EnableOut | BOOL | Enable output. | 
| Dest | DINT | Result of the conversion instruction. Math status flags are set for this output. | 
Description
BCD is the Binary Coded Decimal number system that expresses individual decimal digits (0-9) in a 4-bit binary notation.
| Source | Destination | Destination Type | 
| Negative source < 0 | 0 | |
| Source > 9,999, 999,999, 999,999 | 16#9999_9999_9999_9999 | ULINT | 
| Source > 9,999, 999,999, 999,999 | 16#9999_9999_9999_9999 | LINT | 
| Source > 99,999,999 | 16#9999_9999 | UDINT | 
| Source > 99,999,999 | 16#9999_9999 | DINT | 
| Source > 99,999,999 | 16#9999 | UINT | 
| Source > 99,999,999 | 16#9999 | INT | 
| Source > 99,999,999 | 16#99 | USINT | 
| Source > 99,999,999 | 16#99 | SINT | 
Affects Math Status Flags
| Controllers | Affects Math Status Flags | 
| CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, Compact GuardLogix 5380, and GuardLogix 5580 controllers | Conditional, see . | 
| CompactLogix5370, ControlLogix5570, Compact GuardLogix5370, and GuardLogix5570 controllers | Yes | 
Major/Minor Faults
See  for operand related faults.
| A minor fault will occur if: | Fault type | Fault code | 
| feature is enabled and overflow detected and Source < 0 | 4 | 4 | 
| feature is enabled and overflow detected and Source > 99,999,999 / 9,999, 999,999, 999,999 | 4 | 4 | 
| feature is enabled and overflow detected | 4 | 4 | 
Execution
Ladder Diagram
| Condition/State | Action Taken | 
| Prescan | N/A. | 
| Rung-condition-in is false | N/A. | 
| Rung-condition-in is true | The controller converts the Source to BCD and places the result in the Destination. | 
| Postscan | N/A. | 
Function Block Diagram
FBD Block
| Condition/State | Action Taken | 
| Prescan | N/A | 
| Tag.EnableIn is false. | EnableOut is cleared to false | 
| Tag.EnableIn is true | Dest = the result of computation in BCD value. If overflow occurs Clear EnableOut to false. else  Set EnableOut to true. | 
| Instruction first scan | N/A | 
| Instruction first run | N/A | 
| Postscan | N/A | 
Example
Ladder Diagram

Function Block

Provide Feedback