Proxy
Proxy connection can be configured through the
Connection Settings
Tool.
NOTE:
See FactoryTalk Remote Access Manager Tools for further information on this subject.
You can choose among three proxy types:
- None:No proxy configuration.
- HTTP:The HTTP proxy supports Basic authentication (BA) or no access authentication method.NOTE: Other access authentication methods (for example, DIGEST or NTLM) are not supported.
- SOCKS5:The SOCKS5 proxy does not require any authentication method.NOTE: No access authentication method is supported.
NOTE:
See FactoryTalk Remote Access Manager Tools access and FactoryTalk Remote Access Manager Tools installation for further information on the
Connection Settings
Tool.Provide Feedback