System requirements
Use these system requirements to determine whether your computers can run
FactoryTalk® Optix™
and FactoryTalk Optix Applications
.Hardware requirements for FactoryTalk Optix Studio desktop editor
FactoryTalk Optix Studio desktop editor
For optimal performance of
FactoryTalk Optix Studio desktop editor
, the computer should meet or exceed these hardware requirements: - Intel Core i5 Standard Power processor (i5-8xxx)
- 8 GB of RAM memory
- 20 GB free hard disk space
Software requirements for FactoryTalk Optix Studio desktop editor
FactoryTalk Optix Studio desktop editor
- A supported Windows 10 (x64), Windows 11 (x64), Windows Server 2016, Windows Server 2019, Windows Server 2022 operating system, or Windows Server 2025
- An external code editor to develop custom C# NetLogic codeNOTE:Rockwell Automationrecommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.
Software requirements for FactoryTalk Optix Studio web editor
FactoryTalk Optix Studio web editor
- A web browser that supportsFactoryTalk® Hub™. Supported browsers include modern browsers, such asGoogle Chrome™andMicrosoft Edge®. Older browsers, such asInternet Explorer®, might not function as expected.
Hardware requirements for FactoryTalk Optix Applications
FactoryTalk Optix Applications
Hardware requirements for
FactoryTalk Optix Applications
may vary depending on the application and the type of device that runs
the application.Software requirements for FactoryTalk Optix Applications
FactoryTalk Optix Applications
- A supported Windows 10 (x64), Windows 11 (x64), Windows Server 2016, Windows Server 2019, Windows Server 2022, Windows Server 2025, or Ubuntu 22 (x64) operating system
- FactoryTalk Optix Applicationsare supported on closed Rockwell Automation devices that include OptixPanels and Embedded Edge Compute which run Yocto (ARM64).
NOTE:
FactoryTalk Optix and FactoryTalk Optix Applications can run inside hypervisors such as
VMware® version 15 or higher. For compatibility reasons, software rendering is used by
default.
FactoryTalk Optix Studio and FactoryTalk Optix Applications operating system
supported versions
FactoryTalk Optix Studio
and FactoryTalk Optix Applications
operating system
supported versionsFactoryTalk Optix Studio and FactoryTalk Optix Applications are supported and recommended on
the following versions of Microsoft Windows operating systems, per the standard Rockwell
Automation software policy:
- Windows 10 Enterprise 2019 LTSC 64-bit (v1809)
- Windows 10 Enterprise 2021 LTSC 64-bit (21H2)
- Windows 10 Enterprise IOT 2019 LTSC 64-bit (v1809)
- Windows 10 Enterprise IOT 2021 LTSC 64-bit (21H2)
- Windows 11 Enterprise (Recommended OS, CIS Benchmark)
- Windows 11 Professional (Recommended OS)
- Windows 11 Enterprise 2024 LTSC 64-bit (24H2)
- Windows 11 Enterprise IoT 2024 LTSC 64-bit (24H2)
- Windows Server 2025 Standard (Recommended OS)
- Windows Server 2025 Datacenter (Recommended OS)
- Windows Server 2022 Standard (Recommended OS)
- Windows Server 2022 Datacenter (Recommended OS)
Provide Feedback