Develop a solution for importing UI
Use OPC UA communication to import the UI from another project and display the values of selected variables.
Application example (server and client)
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ImportUI.png/_jcr_content/renditions/original)
TIP:
Download a sample project:
ImportUI.zipPrerequisites
- Create a Server project. See Create a project.
- Create a Client project. See Create a project.
TIP:
The Client project imports data from the Server project.
- To develop the server project
- Arrange the interface elements.
- Save the project.
- To develop the client project
- Arrange the interface elements.
- Save the project.
Application design example (server and client)
![](/content/dam/dita/en/factorytalk-optix/1-03/_images/ImportUIDesign.png/_jcr_content/renditions/original)
In
to run Server and Client projects using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select Run
Provide Feedback