Configure the Date and time configurator widget

Configure the
Date and time configurator
widget to display and edit the system date, time, and time zone manually or through a remote NTP server.
  1. To configure the Date and time configurator widget
  2. Select
    Template Libraries
    .
  3. In
    Libraries
    , select
    Widgets
    .
  4. Under
    Components
    , drag
    Date and time configurator
    into the
    UI
    folder in
    Project view
    .
  5. In
    Libraries
    , select
    Close
    .
  6. In
    Project view
    , in the
    UI
    folder, select the
    DateAndTimeConfigurator (type)
    to display
    Properties
    for the type.
  7. Drag the
    System
    #
    object to
    SystemNode
    in
    Properties
    .
    The system settings are associated with the widget.
  8. At runtime, perform the desired edits, then select
    Apply
    .
  9. Close the application and restart the system for the date and time changes to take effect. See Create a button to restart the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.