Create retentivity storage

Create a retentivity storage data store to retain data of specific project nodes.
For some property values, you can use dynamic links. For more information, see Create dynamic links.
  1. Create the retentivity storage object:
    1. In the
      Project View
      pane, right-click
      Retentivity
      .
    2. Select
      New
      Retentivity storage
      .
    3. (optional) In the
      Properties
      pane, in
      Name
      , select
      Edit
      Edit
      to rename the storage.
  2. Add a project node to retain its data:
    1. In the
      Properties
      pane, next to
      Nodes
      , select
      Add
      Add
      .
    2. (optional) Select
      Edit
      Edit
      to rename the node.
    3. (optional) Expand the node. In
      Kind
      , select Set kind and create a dynamic link.
    4. (optional) Expand the node. In
      NodeClass
      , select the class of the node or select Add dynamic link and create a dynamic link.
  3. Specify how often new data from the selected project nodes is saved by doing one of the following:
    • In
      Write delay
      , enter milliseconds by selecting
      Edit
      Edit
      .
    • In
      Write delay
      , select Add dynamic link and create a dynamic link.
  4. Determine if you want to retain only the changes that are already stored by doing one of the following:
    • In
      Delta observer enabled
      , set the value.
    • In
      Delta observer enabled
      , select Add dynamic link.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.