Recipes editor

The recipes editor widget contains the graphical objects and NetLogic scripts required to display and manage the recipes at runtime.
Use the recipes editor widget to:
  • Display ingredients and values of a stored recipe during editing or loading the controller
  • Create, edit, or delete a recipe
  • Store a recipe in the database
  • Load a recipe from the
    FactoryTalk Optix Application
    to the controller
  • Load a recipe from the controller to the
    FactoryTalk Optix Application

Recipes editor interface

Recipes editor example
Item
Description
A
Recipe name. Assign a name to a new recipe or select an existing recipe.
B
Recipe control buttons.
Save
Store the recipe in the database during editing.
Delete
Delete the selected recipe from the database.
Load
Load the recipe values from the controller to the
FTOptixApplication
.
Apply
Apply the selected recipe on the controller.
C
Recipe schema ingredients.
D
Editable values of the recipe ingredients.
E
Values of the ingredients on the controller.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.