Display content in Project view

To display content of interest in
Project view
, collapse nodes to see only the higher structure of the project or split the view of
Project view
to see different areas of the information model simultaneously.
  • In the
    Project view
    toolbar, select either:
    • Navigate backward
      . Select the previously selected node or item.
    • Navigate forward
      . Select the most recently selected node or item.
  • (optional) Collapse all nodes for easier navigation. Right-click the root project node and then select
    Collapse all
    .
  • (optional) Divide
    Project view
    into two areas that you can scroll separately. Select 
    Split project view
    to divide the view. Select 
    Split project view
    again to remove the division in the view.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.