Delete a node

Delete a node to remove it from the project. Deleting a node removes any references to other nodes. If the deleted node references other nodes, you are prompted to remove all of the references to other nodes.
  1. In
    Project view
    , select the node.
  2. In the view toolbar, select
    Delete
    .
  3. If the node references other nodes, a list of the referenced nodes appears. Select
    Delete
    to confirm the deletion
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.