Create a folder

Create a new folder to contain objects in your project.
  1. In
    Project view
    , select the node to contain the folder. Select the project level node to create a folder at the root level.
  2. In the view toolbar, select
    Add
    new
    or right-click the node, and then select
    New > Folder
    .
The
NewFolder#
appears in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.