Translate a string

Translate a string so that the text for the string can be displayed in different languages.
If no translation is expected for a locale, the string displayed at runtime depends on the fallback locale of the user.
  1. In
    Project view
    , expand
    Translations
    and then double-click a localization library.
  2. Select
    View translation references
    .
  3. In the row of the string to translate, select
    Synchronized
    . A new key with the same name as the string appears in the translation table.
  4. (optional) Rename the key in the
    Translation reference
    page to add a key in the translation table.
    Renaming a key does not remove the key with the previous name.
  5. Select
    View Translation Table
    .
  6. Add translations for the key.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.