Create a localization dictionary

Create a localization dictionary to display application content in the language where the user is located. The localization dictionary contains all of the translated strings in the different languages. You can then select a language to display for the application at both design time and runtime.
If you create a project in
FactoryTalk Optix Studio
using a standard template, the
Translations
folder contains a localization dictionary by default.
  • In
    Project view
    , right-click
    Translations
    and then select
    New
    LocalizationDictionary
    .
The
LocalicationDictionary#
appears in the
Translations
folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.