Complex Dynamic Link Editor
The
Complex Dynamic Link Editor
allows you to add advanced logic to the source node value. The
Complex Dynamic Link Editor
contains:
Item | Description |
---|---|
1 | The path to the variable set by the dynamic link. |
2 | A block diagram that depicts the flow of transformations carried out by dynamic links and the converters which calculate the value of the parent node. |
3 | Dynamic link direction sets the direction between the blocks. The direction changes as you select the icon:
|
4 | Use ![]() You can use this to add additional processing on an output of another block. For example, you can multiply the result of an ExpressionEvaluator by constant values. |
5 | Use ![]() Use to link the source variable to a specific index of the parent variable. to create a
Use to create a converter on which you can dynamically build the variable source path. These options are for engineering units of measure only:
|
6 | Use ![]() |
7 | Use ![]()
|
Provide Feedback