Alarm log grids

FactoryTalk Optix Studio
offers two types of alarm log grids.
  • Alarm log grid
    . Displays a log of alarm events recorded in a database by an event logger such as the Alarm events logger. The Alarm log grid displays alarm information and alarm status in a table. Every row in the table corresponds to a change in alarm status.
  • Alarm log grid with filter
    . Displays the logged data in the same manner as the Alarm log grid, but allows you to temporarily filter the alarms.
An example alarm grid may display the following columns of information:
The default columns in an alarm grid include:
Column
Description
Timestamp
Date and time the alarm event was last updated
Name
Name of the alarm object that generated the alarm event
Source variable
Monitored variable
Message
Message associated with the alarm event
Active
= alarm inactive
= alarm active
Acknowledged
: alarm not acknowledged
: alarm acknowledged
Confirmed
: cause of alarm not addressed
: cause of alarm addressed
Severity
Level of severity of the alarm, from 1 to 1000
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.