System requirements

Use these system requirements to determine whether your computers can run
FactoryTalk Optix Studio
and
FactoryTalk Optix Applications
.

Hardware requirements for
FactoryTalk Optix Studio

For optimal performance of
FactoryTalk Optix Studio
, the computer should meet or exceed these hardware requirements.
  • Intel Core i5 Standard Power processor (i5-8xxx)
  • 8 GB of RAM memory
  • 20 GB free hard disk space
FactoryTalk Optix Studio
and
FactoryTalk Optix Applications
can run inside hypervisors like
VMware®
(version 15 or higher). For compatibility reasons, software rendering is used by default.

Hardware requirements for
FactoryTalk Optix Applications

Hardware requirements for
FactoryTalk Optix Applications
may vary depending on the application and the type of the device that runs the application.

Minimum software requirements for
FactoryTalk Optix Studio desktop version

Microsoft Windows 10 (x64)
An external code editor to develop custom C# NetLogic code
We recommend using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor.

Minimum software requirements for
FactoryTalk Optix Studio web version

A web browser that supports
FactoryTalk Hub
.

Operating system

Microsoft Windows 10 (x64)
Linux Ubuntu 22 (x64)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.