Configure the main window

The main window contains all graphical elements displayed at design time in
FactoryTalk Optix Studio
and at runtime in your
FactoryTalk Optix Application
.
  1. In
    Project view
    , expand
    UI
    and double-click
    MainWindow (type)
    .
    The main window area displays in the editor. The main window does not contain any graphical elements.
  2. In
    Properties
    , set
    Width
    to
    1080
    and
    Height
    to
    600
    .
    The initial dimensions of the main window are now
    1080 x 600
    . At runtime, you can resize the main window at any time. For more information about sizing, see Size conventions.
    TIP: To make the application fit your screen resolution, you can set different
    Width
    and
    Height
    values. Alternatively, you can set
    Full screen
    to
    True
    , however; it is easier to develop and preview applications with the default
    False
    settings.
    Blank resized main window in the editor
  3. (optional) If you want your application window to always float above other windows, set
    Always on Top
    to
    True
    .
  4. (optional) Set
    Caption
    to provide a custom title for your application window.
    For example, set
    Caption
    to
    Quick start application
    to replace the default window title.
Blank main window with a custom caption
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.