Configure a logo

Add and position a logo of your choice in the right corner of the main window.
Prerequisites
Obtain a
PNG
or
SVG
logo of your choice or download a sample logo: ra_logo.svg.
  1. Add the logo
  2. In
    Project view
    , double-click
    MainWindow (type)
    .
  3. Drag the logo file from your computer into the main window area in the editor.
    The logo appears in the editor. Depending on the logo resolution and the main window resolution, the logo might take too much space or be positioned incorrectly.
  4. Position the logo
  5. In
    Properties
    , set
    Width
    to
    200
    .
  6. Set
    Horizontal alignment
    to
    Right
    .
  7. Set
    Top margin
    and
    Right margin
    to
    5
    .
Main window with a logo in the corner
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.