Quick start: develop a sample project

Develop, compile, and run a sample HMI
FactoryTalk Optix Application
that demonstrates different capabilities of
FactoryTalk Optix Studio
.
TIP:
  • At any point of this tutorial, you can test your application by selecting
    Run
    Run
    to run your project using the client emulator on your development computer. For more information, see Deploy a FactoryTalk Optix Application.
  • Throughout this tutorial, save changes periodically by pressing
    S
    or selecting Save from the toolbar.
    You can use Git to version-control your project. For more information, see Version control.
  • You can download, unzip, and open the finished project to investigate its components and settings: QuickStart.zip
Prerequisites
  1. To develop the project
  2. Configure and brand the main window:
    Blank main window with a custom title and logo
  3. Configure panels and tab-based navigation:
    Navigation panel with blank panels
  4. Configure dynamic graphic objects:
    Page1 panel with dynamic graphic objects
  5. Configure variables and add temperature controls:
    Page1 panel with dynamic graphic objects and temperature controls
  6. Configure recipes:
    Page4 panel with recipes editor
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.