Types panel
Types are models of objects or variables from which other objects or variables are derived.
Types panel
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/type_view_callout_c1.png/_jcr_content/renditions/original)
Types are organized into folders by category of object. To add an instance of an object to your project, browse to the object in the folder and then drag it into the object editor canvas.
Provide Feedback