Output panel
The
Output
panel contains buttons to perform tasks on the panel. Button | Function |
---|---|
![]() | Select to display or hide the error messages of maximum severity. |
![]() | Select to display or hide the error messages of minimum severity. |
![]() | Select to display or hide information messages. |
![]() | Select to display or hide verbose 1 messages. |
![]() | Select to display or hide verbose 2 messages. |
![]() | Open the output logs folder. For more information, see System log |
![]() | Delete all messages, regardless of display selected, from the output panel.
TIP:
Messages are not deleted from the log files.
|
Column Name | Description |
---|---|
- | Message severity level ![]() ![]() ![]() |
Code | (Only for FactoryTalk Optix predefined messages) Message ID code. |
Timestamp | The time the system logged the message. |
Category | Category of the FactoryTalk Optix Platform message or module that generated the message. |
Object | The element referenced by the message, if applicable. |
Message | Message content. |
TIP:
Select the arrow
in a column heading to sort messages in ascending or descending order according to the data in that column.
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/timestamp_sort_arrow.png/_jcr_content/renditions/original)
In the
to filter the displayed messages by category.
Category
column, select Provide Feedback