Scroll view example

Use this object to provide a panel that includes scroll bars, so that it can contain content larger than the panel itself.
TIP:
Scroll view
supports:
  • Touch and multitouch gestures, such as pan or pinch-to-zoom.
  • Keyboard and mouse operation, such as the
    combination to zoom-in or zoom-out.
Scroll view example

Use case

Display overview information, drawings, or other items that are larger than the main application container.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.