OPC UA server example

Use this object to publish project nodes to the OPC UA client project.

Use case

Publish the selected project nodes to the selected users through the OPC UA client.
TIP: The OPC UA server publishes all child nodes and all parent nodes of the selected nodes. Multiple clients can connect to a single server endpoint.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.