Linear gauge example

Use this object to set and display a whole number value within a range of possible values.
Linear gauge example
Animated image of a linear gauage moving between values of 0 to 100

Use case

Set or display the value of an analog variable within a minimum and maximum value.
TIP: Use the
Tooltip
property to show or hide the display of the value above the selection point on the gauge. Use the
Warning zone
property to display specific ranges of values in different colors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.