Dropdown button example

Use this object to open or close a panel when a Button is selected.
Dropdown button example
animated image that shows a content panel being displayed when the button is clicked

Use case

Open a panel that contains additional options or information when you select a Button.
TIP: If there is not enough space in width or height with respect to the set opening direction, the panel is opened in the opposite direction.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.