Button example

Use this object to run methods at runtime. Buttons can contain text or an image.
Button example
Three button controls with different styles applied.
graphic showing three different button styles

Events

You can trigger methods with
Button
objects by using these events:
Event
Generated at runtime when
MouseClick event
An object is clicked or touched and then released.
MouseDown event
An object is clicked or touched.
MouseUp event
The click or touch of the object is released.

Use case

Trigger different actions, for example:
  • Start report generation.
  • Acknowledge active alarm.
  • Signal an emergency condition.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.