Advanced SVG image

Use this object to display an SVG Tiny 1.2 image and change the properties of individual image parts at design time or runtime.
Application example - disabled alarm
Application example - enabled alarm

Use case

Statically or dynamically modify a part or the entire SVG image. For example, signal a hardware part malfunction by highlighting a given hardware component representation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.