Create a login form
Create an interface that allows for logging in.
- Add a preconfigured widget (type):
- In the toolbar, select.
- InLibraries, search forLogin form.
- UnderComponents, dragLogin formonto theUIfolder in theProject viewpane.
- InProject view, right-clickMainWindow (type)and select .
- InProperties, create a dynamic link betweenUsersand .For more information about dynamic links, see Create dynamic links.
Provide Feedback