Develop buttons for closing the application and shutting down the host system
Create a check box that shows or hides a clock label, which state is persistent based on the currently logged in user.
IMPORTANT:
Pressing the
Shut down system
button immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing the button will immediately shut down your Windows system.Application example
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/CloseApplicationShutDownSystem.png/_jcr_content/renditions/original)
TIP:
Download a sample project:
ExampleApplication-CloseApplicationShutDownSystem.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example
![](/content/dam/dita/en/factorytalk-optix/1-00/_images/CloseApplicationShutDownSystemDesign.png/_jcr_content/renditions/original)
In
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
FactoryTalk Optix Studio
, select ![Run](/content/dam/dita/en/factorytalk-optix/1-00/_images/toolbar_run_icon.png/_jcr_content/renditions/original)
Provide Feedback