FactoryTalk Hub Menu

The
Hub Portal Menu
is divided into two sections, Hub Manager and Organization. Hub manager features require that you be an owner or administrator of an organization.
Hub Manager
provides access to the following features:
  • Manage User Access
    : View, add, and remove access for various Users.
  • View Entitlements
    : Entitlements add different apps to your organization. The service provided is tied to a contract number and has a defined start date and expiry date.
  • Invite Users
    : Send an invitation email to a new User.
  • Approve Users
    : Approve Users who have requested to join your organization.
  • Manage Organizational Invites:
    View the status of invitations sent for your organization.
Organization
provides access to the following features:
  • Create Organization
    : Create an organization. Organizations are collections of applications, users, and resources that can be accessed and managed using FactoryTalk Hub.
  • Edit Organization:
    Edit an existing organization
  • Join Organization
    : Join an existing organization.
  • Universal Credits Balance:
    Allows you to see the status and balance of your universal credits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.