Process Solutions
Device Integration
Field Device Testing Procedures
The Interoperability testing procedures below are followed for each field device and the results recorded in a test report for integration planning purposes.- Install the Third Party Device in an operating H1 network.
- Change the BOF Class of the device.
- Assign a tag to the device.
- Add function blocks to device.
- Perform download operations.
- Set device to factory defaults.
- Configure function blocks.
- Export tags.
- Create a Control Module and add function blocks and links to the Linking Device.
- Verify device operation — monitor link values.
- Verify device operation — UPDATE Command.
- Verify that a device can bridge across H1 channels in the same FFLD.
- Verify that a device will operate with the AB CN2FF module.