Machine Builder (OEM) Solutions

Subscribe Now

Machine Builder (OEM) Solutions

What Matters

Standards Matter

Machine builders and manufacturers are both battling to maintain a competitive edge in the market.While the end goal is the same, the two have distinct areas of concentration. OEMs want to manage the cost of engineering time and build scalable machines to address changing functional specifications. Meanwhile, manufacturers want equipment that easily ties to upstream and downstream operations, and operates with limited engineering resources.

Using Programming Standards to Align OEM and End-User Goals

Industry programming standards play an important role in helping both OEMs and end users achieve their goals. By providing a common, efficient framework that addresses every phase of the automation life cycle, programming standards help end users speed installation and startup as well as reduce the total cost of ownership.

Modular programming standards give OEMs a basic framework for development, and create an environment where programmers can reuse definitions, structures and lines of code. This structured, reusable model applies proven software objects from machine to machine, accelerating program development and providing design consistency when multiple programmers are involved during machine design.

Leveraging modular programming standards allow machine designers to spend less time coding and more time adding value to their machine solutions. This is particularly important considering program development typically is the most time-consuming, costly, and riskiest stage of machine design. Overall, shorter design time translates into lower engineering costs, faster time to market, and higher margins.

When it comes time to install the machine, common design practices help streamline the installation process, especially for multi-plant installations. Maintenance and troubleshooting tasks also are easier since operators and technicians are familiar with the code modules.

As industry programming standards continue to evolve to keep pace with advancements in automation technology, these standards play an important role in helping OEMs and end users meet performance and efficiency goals. Building machines and processes on a common technology framework offers more people access to the underlying systems. It also allows automation to evolve in an orderly fashion as new devices and software become available.

Product and Services Highlights

Rockwell Automation offers a wide range of tools to help OEMs bring commonality to technology. They include: