Condition Monitoring Solutions
Software
Emonitor® — Asset Health Analysis/Intelligent Advisory
Emonitor constructs a diagnostic model of the plant machinery based on the mechanical design information, such as bearing information, shaft configuration, gear design, fan blade design or motor data. Emonitor includes a reference database of over ten thousand bearings to facilitate this task. The condition monitoring analyst can diagnose problems interactively or automatically using the powerful Intelligent Advisory Decision module. The Emonitor analysis captures the important data by recording the symptoms, diagnosis, and severity for the event.